FB#.SCALED.P
Description
FB#.SCALED.P is the scaled feedback position. See Scaled Feedback for details on the calculation.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-01-000 |
General Information
|
Type |
Read Only |
|
Units |
Depends on FB#.SCALED.PIN and FB#.SCALED.POUT |
|
Range |
Full position range |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
|
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.